Start data transfer by the end of A/D conversion.
(Get A/D conversion results of 4 pins and copy them to RAM. Then, calculate the average of the results.)
[GUI setting example]
| 
 DMA controller  | 
 Used  | |||
| 
 DMA0  | 
 Used  | |||
| 
 DMAoperation setting  | 
 Used  | |||
| 
 Transfer direction setting  | 
 SFR to internal RAM  | |||
| 
 Transfer data size setting  | 
 8 bits  | |||
| 
 SFR address  | 
 ADCR - 0x000fff1e  | |||
| 
 RAM address  | 
 0xffe00  | |||
| 
 Transfer byte count  | 
 4  | |||
| 
 Trigger signal  | 
 INTAD (Please set INTAD)  | |||
| 
 DMA0 transfer end interrupt (INTDMA0)  | 
 Used  | |||
| 
 Priority  | 
 Low  | |||
| 
 A/D convertor  | 
 Used  | |||
| 
 ADC  | 
 Used  | |||
| 
 A/D convertor operation setting  | 
 Used  | |||
| 
 Comparator operation setting  | 
 Operation  | |||
| 
 Resolution setting  | 
 8 bits  | |||
| 
 VREF(+) setting  | 
 VDD  | |||
| 
 VREF(-) setting  | 
 VSS  | |||
| 
 Trigger mode setting  | 
 Software trigger mode  | |||
| 
 Operation mode setting  | 
 Countinous select mode  | |||
| 
 ANI0 - ANI7 analog input selection  | 
 ANI0 - ANI3  | |||
| 
 A/D channel selection  | 
 ANI0 - ANI3  | |||
| 
 Conversion time mode  | 
 Normal 1  | |||
| 
 Conversion time  | 
 34 (1088/fCLK)(μs)  | |||
| 
 Conversion result upper/lower bound value setting  | 
 Generates an interrupt request (INTAD) when ADLL≦ADCRH≦ADUL  | |||
| 
 Upper bound (ADUL) value  | 
 255  | |||
| 
 Lower bound (ADLL) value  | 
 0  | |||
| 
 Use A/D interrupt (INTAD)  | 
 Used  | |||
[API setting example]
r_main.c
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Enable DMA0 transfer */
R_DMAC0_Start();
/* Start the AD converter */
R_ADC_Start();
while (1U)
{
NOP();
}
/* End user code. Do not edit comment generated here */
}
r_cg_dmac_user.c
/* Start user code for include. Do not edit comment generated here */
#include "r_cg_adc.h"
/* End user code. Do not edit comment generated here */
/* Start user code for pragma. Do not edit comment generated here */
#pragma address (g_adc_buf = 0x0ffe00)
/* End user code. Do not edit comment generated here */
/* Start user code for global. Do not edit comment generated here */
volatile uint8_t g_adc_buf[5][4];
volatile uint8_t g_adc_buf_cnt = 0U;
/* End user code. Do not edit comment generated here */
static void __near r_dmac0_interrupt(void)
{
/* Start user code. Do not edit comment generated here */
uint8_t i;
uint8_t j;
uint16_t temp;
/* Stop the AD converter */
R_ADC_Stop();
/* Disable DMA0 transfer */
R_DMAC0_Stop();
/* Change DMA0_RAM address */
if ((++g_adc_buf_cnt) < 4U)
{
DRA0 += 4U;
}
else
{
DRA0 = _FE00_DMA0_RAM_ADDRESS;
g_adc_buf_cnt = 0U;
/* Calculate the average */
for (i = 0; i < 4U; i++)
{
temp = 0U;
for (j = 0; j < 4U; j++)
{
temp += g_adc_buf[j][i];
}
g_adc_buf[4][i] = temp / 4U;
}
}
/* Enable DMA0 transfer */
R_DMAC0_Start();
/* Start the AD converter */
R_ADC_Start();
/* End user code. Do not edit comment generated here */
}