Usage example

Use timer as One-shot timer.

[GUI setting example]

Timer

Used

TAU0

Unused

WUTM

Used

16-bit wake-up timer operation setting

Used

Count clock setting

Auto

Interval value

100ms (Actual value:100)

WUTM and WUTMCMP match, generate an interrupt (INTWUTM)

Used

Priority(INTWUTM)

Low

[API setting example]

r_main.c

void main(void)

{

R_MAIN_UserInit();

/* Start user code. Do not edit comment generated here */

/* Start WUTM counter */

R_WUTM_Start();

while (1U)

{

;

}

/* End user code. Do not edit comment generated here */

}

r_cg_timer_user.c

static void __near r_wutm_interrupt(void)

{

/* Start user code. Do not edit comment generated here */

/* Stop WUTM counter */

R_WUTM_Stop();

/* End user code. Do not edit comment generated here */

}