Usage example

Start clock and buzzer output

[GUI setting example]

Clock output/Buzzer output

Used

PCLBUZ0

Used

Clock output/buzzeroutput operation setting

Used

PCLBUZ0 output clock selection

1.875 (fSL/2^3)(kHz)

Slow mode

Unused

[API setting example]

r_main.c

void main(void)

{

R_MAIN_UserInit();

/* Start user code. Do not edit comment generated here */

/* Start the PCLBUZ0 module */

R_PCLBUZ0_Start();

while (1U)

{

;

}

/* End user code. Do not edit comment generated here */

}