1.1 Overview

The Code Generator, which is one of the components provided by CS+, enables you to output the source code (device driver programs, C source files and header files) necessary to control the peripheral functions (clock generator, port functions, etc.) provided by the microcontroller by configuring various information using the GUI.