-
wup_tsk
iwup_tsk
-
ER wup_tsk (ID tskid);
ER iwup_tsk (ID tskid);
|
|
|
|
|
|
ID tskid;
|
Value: ID number of the task.
|
These service calls cancel the WAITING state (sleeping state) of the task specified by parameter
tskid.
As a result, the target task is moved from the sleeping state to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
If the target task is in a state other than the sleeping state when this service call is issued, this service call does not move the state but increments the wake-up request counter (by added 1 to the wake-up request counter).
Note The wake-up request counter managed by the RI600V4 is configured in 8-bit widths. If the number of wake-up requests exceeds the maximum count value 255 as a result of issuing this service call, the counter manipulation processing is therefore not performed but "E_QOVR" is returned.
|
|
|
|
|
|
|
|
|
|
|
- When iwup_tsk was issued from a non-task, TSK_SELF was specified for tskid.
|
|
|
|
- This service call was issued in the CPU locked state.
- The iwup_tsk was issued from task.
- The wup_tsk was issued from non-task.
- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
|
|
|
|
- Specified task is in the DORMANT state.
|
|
|
|
- Wake-up request count exceeded 255.
|