|
|
Assembles the selected assembler source file.
Note that this menu is only displayed when a system information table file is selected.
Note that this menu is disabled when the build tool is in operation.
|
|
|
Opens the selected file with the application corresponds to the file extension.
Note that this menu is disabled when multiple files are selected.
|
Open with Internal Editor...
|
Opens the selected file with the Editor panel.
Note that this menu is disabled when multiple files are selected.
|
Open with Selected Application...
|
Opens the Open with Program dialog box to open the selected file with the designated application.
Note that this menu is disabled when multiple files are selected.
|
Open Folder with Explorer
|
Opens the folder that contains the selected file with Explorer.
|
|
|
Shows the cascading menu to add files and category nodes to the project.
|
|
|
|
Opens the Add Existing File dialog box to add the selected file to the project.
|
|
|
|
Opens the Add File dialog box to create a file with the selected file type and add to the project.
|
|
|
|
Adds a new category node at the same level as the selected file. You can rename the category.
This menu is disabled while the build tool is running, and if categories are nested 20 levels.
|
|
|
Removes the selected file from the project.
The file itself is not deleted from the file system.
Note that this menu is disabled when the build tool is in operation.
|
|
|
Copies the selected file to the clipboard.
When the file name is in editing, the characters of the selection are copied to the clipboard.
|
|
|
This menu is always disabled.
|
|
|
You can rename the selected file.
The actual file is also renamed.
|
|
|
|