4.2.4.1 Allocation of function and data to section

The CC-RH controls allocation to memory or the access method by allocating functions or data to sections.

-

Sections for functions

Table 4.15

Types of Sections for Functions

Section Relocation Attribute

Default Section Name

Access Method

Alignment Condition

text

.text

32-bit relative mode from r0

2

pctext

.pctext

32-bit relative mode from PC

-

The .text section is used by default.

This section cannot be used by the PIC facility.

-

The .pctext section is a section to be used by the PIC facility.

 

-

R0-relative sections for data

Table 4.16

Types of R0-Relative Sections for Data

Section Relocation Attribute

Default Section Name

Data to be Allocated

Access Method

Alignment Condition

zdata

.zdata

Variables with initial value

16-bit relative mode from r0

4

zbss

.zbss

Variables with no initial value

zdata23

.zdata23

Variables with initial value

23-bit relative mode from r0

zbss23

.zbss23

Variables with no initial value

data

.data

Variables with initial value

32-bit relative mode from r0

bss

.bss

Variables with no initial value

-

The .data and .bss sections are used by default.

-

The .zdata, .zbss, .zdata23, and .zbss23 sections are used for access in a short instruction length.

-

Any of the R0-relative sections cannot be used by the PID facility.

 

-

EP-relative sections for data

Table 4.17

Types of EP-Relative Sections for Data

Section Relocation Attribute

Default Section Name

Data to be Allocated

Access Method

Alignment Condition

tdata4

.tdata4

Variables with initial value

4-bit relative mode from r30 (EP)

The sld or sst instruction can be used.

4

tbss4

.tbss4

Variables with no initial value

tdata5

.tdata5

Variables with initial value

5-bit relative mode from r30 (EP)

The sld or sst instruction can be used.

tbss5

.tbss5

Variables with no initial value

tdata7

.tdata7

Variables with initial value

7-bit relative mode from r30 (EP)

The sld or sst instruction can be used.

tbss7

.tbss7

Variables with no initial value

tdata8

.tdata8

Variables with initial value

8-bit relative mode from r30 (EP)

The sld or sst instruction can be used.

tbss8

.tbss8

Variables with no initial value

edata

.edata

Variables with initial value

16-bit relative mode from r30 (EP)

ebss

.ebss

Variables with no initial value

edata23

.edata23

Variables with initial value

23-bit relative mode from r30 (EP)

ebss23

.ebss23

Variables with no initial value

edata32

.edata32

Variables with initial value

32-bit relative mode from r30 (EP)

ebss32

.ebss32

Variables with no initial value

-

The .tdata* and .tbss* sections are used for access in a short instruction length.

The sld or sst instruction which is even shorter can be used.

These sections can be used even by the PID facility.

-

The .edata, .ebss, .edata23, and .ebss23 sections are used for access in a short instruction length.

These sections can be used even by the PID facility.

-

The .edata32 and .ebss32 sections are sections to be used by the PID facility.

 

-

GP-relative sections for data

Table 4.18

Types of GP-Relative Sections for Data

Section Relocation Attribute

Default Section Name

Data to be Allocated

Access Method

Alignment Condition

sdata

.sdata

Variables with initial value

16-bit relative mode from r4 (GP)

4

sbss

.sbss

Variables with no initial value

sdata23

.sdata23

Variables with initial value

23-bit relative mode from r4 (GP)

sbss23

.sbss23

Variables with no initial value

sdata32

.sdata32

Variables with initial value

32-bit relative mode from r4 (GP)

sbss32

.sbss32

Variables with no initial value

-

The .sdata, .sbss, .sdata23, and .sbss23 sections are used for access in a short instruction length.

These sections can be used even by the PID facility.

-

The .sdata32 and .sbss32 sections are sections to be used by the PID facility.

 

-

Sections for constant data

Table 4.19

Types of Sections for Constant Data

Section Relocation Attribute

Default Section Name

Data to be Allocated

Access Method

Alignment Condition

zconst

.zconst

const variables

String literal

Initial values of auto variablesNote 1

16-bit relative mode from r0

4

zconst23

.zconst23

23-bit relative mode from r0

const

.const

32-bit relative mode from r0

pcconst16

.pcconst16

16-bit relative mode from the __pc_data symbol

pcconst23

.pcconst23

23-bit relative mode from the __pc_data symbol

pcconst32

.pcconst32

32-bit relative mode from the __pc_data symbol

Note 1.

The initial values of auto variables are in the .const section when the PIROD facility is not used and are in the .pcconst32 section when the PIROD facility is used. In either case, they cannot be changed.

-

The .const section is used by default.

This section cannot be used by the PIROD facility.

-

The .zconst and .zconst23 sections are used for access in a short instruction length.

These sections cannot be used by the PIROD facility.

-

The .pcconst16, .pcconst23, and .pconst32 sections are sections to be used by the PIROD facility.

 

The sections to which the CC-RH allocates functions or data are the four sections .text, .data, .bss, and .const, by default.

The longer the relative distance at access is, the access is in a long instruction length and the code size is increased.

 

The CC-RH can allocate functions and data to desired sections using the extended facilities. This makes it possible to generate code using the relocation attribute characteristics of each section.

 

(1)

#pragma section directive

Describe the #pragma section directive in the following format.

#pragma section attribute-strings "user-defined-name"
#pragma section attribute-strings
#pragma section user-defined-name
#pragma section default
or
#pragma section

 

Section relocation attributes are specified using "attribute strings", and section names are specified using "user-defined names". The usable attribute strings vary depending on the specified options.

The relationship between specifiable attribute strings, corresponding section relocation attributes, and options that can be specified as conditions is shown in Table 4.20.

Attribute strings are case-sensitive.

Table 4.20

Relationship between Attribute Strings and Section Relocation Attributes

Attribute String

Section Relocation Attribute

Specifiable Condition

text

text

When -pic is not specified

pctext [V1.07.00 or later]

pctext

When -pic is specified

r0_disp16

zdata/zbss

When -pid is not specified

r0_disp23

zdata23/zbss23

r0_disp32

data/bss

ep_disp4

tdata4/tbss4

When -Xep=fix is specified

ep_disp5

tdata5/tbss5

ep_disp7

tdata7/tbss7

ep_disp8

tdata8/tbss8

ep_disp16

edata/ebss

ep_disp23

edata23/ebss23

ep_disp32 [V1.07.00 or later]

edata32/ebss32

When -Xep=fix and -pid are both specified

gp_disp16

sdata/sbss

When -r4=fix is specified

gp_disp23

sdata23/sbss23

gp_disp32 [V1.07.00 or later]

sdata32/sbss32

When -r4=fix and -pid are both specified

zconst

zconst

When -pirod is not specified

zconst23

zconst23

const

const

pcconst16 [V1.07.00 or later]

pcconst16

When -pirod is specified

pcconst23 [V1.07.00 or later]

pcconst23

pcconst32 [V1.07.00 or later]

pcconst32

 

The following characters are usable in user-defined names.

-

0 to 9

-

a to z, A to Z

-

_

-

@

-

.

 

The allocation section of functions or data written after a #pragma section directive is determined in accordance with the following rules.

1. The relocation attribute is determined from the "attribute string".

(1) For data, *data* or *bss* is automatically selected depending on whether there is an initial value.

(2) A format with no attribute string has an effect on both functions and data, and the default relocation attribute of the compiler is used.

2. A string representing the relocation attribute is linked after the "user-defined name"Note.

(1) If the user-defined name starts with a number from 0 to 9, "_" is added to the beginning.

(2) If there is no user-defined name, the default section name is used without change.

Note

This is to prevent sections with different section relocation attributes from having the same section name.

3. When the format of #pragma section default or #pragma section is specified, it has an effect on both functions and data, and the default relocation attribute of the compiler and the default section name are used.

 

A #pragma section directive is valid from the position where it was written up to the position where the next #pragma section directive appears or up to the end of the source file.

Example

#pragma section gp_disp16 "foo"
int a = 1;        /* foo.sdata */
int b;            /* foo.sbss */
 
#pragma section zconst23 "bar"
const int c = 2;  /* bar.zconst23 */
 
#pragma section text "123"
void func() {}    /* _123.text */
 
#pragma section baz
int d = 3;        /* baz.data */
int e;            /* baz.bss */
const int f = 4;  /* baz.const */
void func2() {}   /* baz.text */
 
#pragma section default
int g = 3;        /* .data */
int h;            /* .bss */
const int i = 4;  /* .const */
void func3() {}   /* .text */

 

The effect of a #pragma section directive differs between variables and functions.

-

Variable

If there are multiple declarations and definitions for a variable and a different #pragma section directive is specified for each, the #pragma section directive that appears first is valid.

Example

int x = 1;    /* Variable x is allocated to foo.data */
int y = 2;    /* Variable y is allocated to bar.data */
 
#pragma section foo
extern int x;
 
#pragma section bar
extern int x;
extern int y;

-

Function

When the -pic option is not specified, #pragma section is valid only for function definitions.

When the -pic option is specified, similar as to variables, #pragma section is valid for both declarations and definitions.