2.6 Specifying Multiple Options

This section describes the operation when two or more options are specified for the ccrl command at the same time.

 

Note the following when specifying multiple options by using -subcommand or -asmopt.

-

When a file is specified through the -subcommand option, the options in the file are expanded at the location where the -subcommand option is specified on the command line. Therefore, the rules described in this section are applied to the options and location after expansion.

-

When options are specified through any of -asmopt, -lnkopt, -asmcmd, and -lnkcmd, the specified options are not expanded on the command line. Therefore, the rules described in this section are not applied to these options.