3.2.11 CRC information

When the -crc option is specified, the CRC operation result and its output address is output.

The output example of the CRC information is shown below.

***CRC Code***
CODE:    cbob       (1)
ADDRESS: 00007ffe   (2)

Number

Description

(1)

CRC operation result

The CRC operation result is output.

(2)

Address of CRC operation result output

The address of CRC operation result output is output.