^


Obtains the exclusive OR operation for each bit of the first and second term values.

[Function]

Performs an Exclusive-OR operation between the value of the 1st term of an expression and the value of its 2nd term on a bit-by-bit basis and returns the result.

[Application example]

MOV     A, #0x9A ^ 0x9D         ; (1)

(1)

XOR operation is performed between the two values "0x9A" and "0x9D" as follows:
This operation loads "0x07" in the A register.