5.2.5 External definition/External reference directives

External definition, external reference directives clarify associations when referring to symbols defined by other modules.

This is thought to be in cases when one program is written that divides module 1 and module 2. In cases when you want to refer to a symbol defined in module 2 in module 1, there is nothing declared in either module and and so the symbol cannot be used. Due to this, there is a need to display "I want to use" or "I don't want to use" in respective modules.

An "I want to refer to a symbol defined in another module" external reference declaration is made in module 1. At the same time, a "This symbol may be referred to by other symbols" external definition declaration is made in module 2.

This symbol can only begin to be referred to after both external reference and external definition declarations in effect.

External definition, external reference directives are used to to form this relationship and the following instructions are available.

Table 5.21

External Definition/External Reference Directives

Directive

Overview

.PUBLIC

Declares to the optimizing linker that the symbol described in the operand field is a symbol to be referenced from another module

.EXTERN

Declares to the optimizing linker that a symbol in another module is to be referenced in this module

.EXTBIT

Declares to the optimizing linker that a bit symbol in another module is to be referenced in this module