11.4.3 Overwrite of variable/function information file

After the variable/function information file that was output by the -vfinfo option specification is edited, specifying the same file name in the -vfinfo option at the second linkage will overwrite the variable/function information file.

Save the edited variable/function information file under another name, do not specify the -vfinfo option after the file has been edited, or change the output file name of the -vfinfo option.