div


Perform division of int type to obtain the quotient and remainder

[Classification]

Standard library

[Syntax]

#include <stdlib.h>

div_t __far div(int numer, int denom);

[Return value]

The structure holding the result of the division is returned. When divided by 0, -1 is set as quotient quot and numer is set as remainder rem.

[Description]

This function is used to divide a value of int type.

This function calculates the quotient (quot) and remainder (rem) resulting from dividing numerator numer by denominator denom, and stores these two integers as the members of the following structure div_t.

typedef struct {
        int quot;
        int rem;
} div_t;

 

When the value cannot be divided, the quotient of the result becomes an integer that is closest to the algebraical quotient and has a smaller absolute value than it.