7.5.7 Standard I/O functions
Standard I/O functions are as follows.
Table 7.9 | Standard I/O Functions |
|
|
|
|
printf
|
Write text in specified format to SFR
|
|
scanf
|
Read text in specified format from SFR
|
|
snprintf [V1.07 or later]
|
Write text in specified format to array (C99)
|
|
sprintf
|
Write text in specified format to array
|
|
sscanf
|
Read text in specified format from character string
|
|
vprintf
|
Write text in specified format to SFR
|
|
vsnprintf [V1.07 or later]
|
Write text in specified format to array (C99)
|
|
vsprintf
|
Write text in specified format to array
|
|
getchar
|
Read one character from SFR
|
|
gets
|
Read character string from SFR
|
|
putchar
|
Write one character to SFR
|
|
puts
|
Write character string to SFR
|
|
perror
|
Error processing
|
Specifications are implemented, so that in each function, input from stdin is performed through the getchar function and output to stdout is performed through the putchar function.
To change stdin and stdout, replace the getchar function and putchar function, respectively.
Output to stderr in the perror function is the same as output to stdout, and so it is performed through the putchar function. Note that replacing the putchar function will also change stderr. To change the output destination of stderr to something other than stdout, replace the perror function