1.2 Special Features

CC-RL is equipped with the following special features.

(1)

Language specifications in accordance with C90 and C99 standards.

The C language specifications conform with the C90 and C99 standards.

(2)

Advanced optimization

Advanced optimization including global program optimization is applied.

This yields smaller and faster code.

(3)

High portability

The industry-standard ELF format is used for object code. In addition, the industry-standard DWARF2 or DWARF3 format is used for debugging information.

(4)

Multifunctional

Static analysis and other functionality is provided via linking between Renesas Electronics and partner tools.