6.1 Sections

A section is the basic unit making up programs (area to which programs or data are allocated). For example, program code is allocated to a text-attribute section and variables that have initial values are allocated to a data-attribute section. In other words, different types of information are allocated to different sections.

Section names can be specified within source file. In C language, they can be specified using a #pragma section directive and in assembly language they can be specified using section definition directives.

Even if the #pragma directive is not used to specify a section, however, allocation by the compiler to a particular section may already be set as the default setting in the program code or data (variables).