3.1.5
Assembler Command Specification Information
The file names and options specified on the command line when the assembler is invoked are output. The assembler command specification information is output at the end of the list file. The following figure shows an example of command specification information output.
Cpu Type (1)
-ISA=RXV1
Command Parameter (2)
-output=sample.obj
-nologo
-listfile=sample.lst
|
|
|
|
Microcomputer selected for the assembler
|
|
File names and options specified for the assembler
|