(1) | When the file name and line number are included |
file-name (line-number) : message-type component-number message-number : message
|
(2) | When the file name and line number aren't included |
message-type component-number message-number : message
|
Remark | Following contents are output as the continued character string. |
MESSAGE TYPES : 1 alphabetic character
COMPONENT NUMBERS : 05
MESSAGE NUMBERS : 5 digits