This dialog box is used to configure action events (see "2.17 Set an Action into Programs").
This dialog box appears only when connected to the debug tool.
| Also see "2.18.6 Notes for setting events" for details on Printf events (e.g. limits on the number of enabled events). | 
 
This section describes the following.
| On the Editor panel, move the caret to the line where you wish to set an action event, then select [Register Action Event...] from the context menu. | 
| On the Disassemble panel, move the caret to the address where you wish to set an action event, then select [Register Action Event...] from the context menu. | 
| On the Events panel, select an action event, then select [Edit Condition...] from the context menu. | 
Select a tab to switch the type of an action event to be set.
This dialog box has the following two tabs.
| If this dialog box is opened by selecting [Edit Condition...] from the context menu, this area does not appear. | 
Use this area to configure detailed condition of an action event.
For details on how to setup an action event, see the section explaining the corresponding tab.