To delete a Timer Result event you have set, on the Editor panel/Disassemble panel, right-click the event mark in the event area and select [Delete Event] from the context menu that is displayed.
Also, there is another way to delete a set event.  Select the Timer Result event you want to delete on the Events panel, and then click the 
 button in the toolbar (see "2.18.4  Delete events").