2.6.2.2  
Change display format
 
The display format of the disassemble area can be changed using buttons below on the toolbar. 
| 
 
View 
 | 
 
The following buttons to change the display format are displayed.  
 | 
| 
 
  
 | 
 
 
Show Offset 
 | 
 
Displays the offset value of the label. The offset value from the nearest label is displayed when a label is defined for the address.  
 | 
| 
 
 
Show Symbol 
 | 
 
Displays the address value as the result of disassembling in the format "symbol + offset value" (default).   
Note that when a symbol has been defined as the address value, only the symbol is displayed.   
 | 
| 
 
 
Show Function Name 
 | 
 
Displays the name of the register by its function name (default).   
 | 
| 
 
 
Show Absolute Name 
 | 
 
Displays the name of the register by its absolute name.   
 |