2.11.7  
Clear the trace memory
 
To clear the collected trace data contents, click the  button on the toolbar.
 button on the toolbar. 
Note that this button is disabled while a tracer is running. 
| 
Remark 1. | [IECUBE][Simulator]When [Yes] is specified in the [Clear trace memory before running] property in the [Trace] category on the [Debug Tool Settings] tab of the Property panel, the trace memory is cleared each time a program is executed.
 | 
| 
Remark 2. | [E1][E20][EZ Emulator]The trace memory is cleared each time a program is executed (fixed).
 |