2.10.1.1
Change display format of values
The display format of this panel can be changed using buttons below on the toolbar.
Note that these buttons are disabled during execution of a program.
|
Notation
|
The following buttons to change the notation of a data value are displayed.
|
|
|
AutoSelect
|
Displays values on this panel in the default notation according to the type of variable (default).
|
|
Hexadecimal
|
Displays values on this panel in hexadecimal number.
|
|
Decimal
|
Displays values on this panel in decimal number.
|
|
Octal
|
Displays values on this panel in octal number.
|
|
Binary
|
Displays values on this panel in binary number.
|
|
Encoding
|
The following buttons to change the encoding of character variables are displayed.
|
|
|
ASCII
|
Displays character variables in ASCII code (default).
|
|
Shift_JIS
|
Displays character variables in Shift_JIS code.
|
|
EUC-JP
|
Displays character variables in EUC-JP code.
|
|
UTF-8
|
Displays character variables in UTF-8 code.
|
|
UTF-16
|
Displays character variables in UTF-16 code.
|