2.13.6.1
Changing the display mode
By clicking one of the toolbar buttons shown below, it is possible to change the display mode as suitable for the purpose of use.
However, these buttons are disabled while the trace function is in operation.
Table 2.14 | Trace Panel Display Modes |
|
|
|
|
|
|
Mixed display mode
|
Instructions (disassemble), label names, source text (corresponding source lines), and point trace results are displayed (default).
|
|
|
Disassemble display mode
|
Instructions (disassemble), label names, and point trace results are displayed.
|
|
|
Source display mode
|
Source text (corresponding source lines) are displayed.
However, if any place that has no debug information is executed, a notice "<No Debug Information>" is displayed.
|
Figure 2.147 | Example of Source Display Mode (Trace Panel) |