1.2 Features

The following are the editor features provided by CS+.

Caution

C++ source files are only supported by CC-RX.

 

-

Display and editing of the contents of files
The contents of text files and C/C++ source files can be displayed/edited.


-

Support of the code outlining
For a C/C++ source file, this function allows you to expand and collapse source code blocks so that you can concentrate on the areas of code which you are currently modifying or debugging.


-

Mixed display of C/C++ source text and disassembled text
By connecting to the debug tool, the C/C++ source text and the disassembled text can be displayed together on the same panel.


-

Source level debugging and instruction level debugging
By connecting to the debug tool, the C/C++ source file can be debugged either at the source or the instruction level.


-

Display of the code coverage measurement result
By connecting to the debug tool that supports the coverage function, the code coverage measurement result can be displayed.