When hovering the mouse cursor over a variable in the source text, a pop-up that shows the name and value of the variable is displayed ("<variable name>=<variable value>").
The display format of the variable value is same as the display format of watch expressions depending on the type of the variable.
| This function is enabled only when connected to the debug tool and the downloaded source file is opened in this panel. |