project.GetFunctionList


This function displays the list of the functions of the active project.

[Specification format]

project.GetFunctionList(fileName = "")

[Argument(s)]

Argument

Description

fileName

Specify the full path of the file that the list of the functions are displayed (default: not specified).

[Return value]

List of function information (see the FunctionInfo property for detail)

[Detailed description]

-

This function displays the list of the functions of the active project shown by the following format.

function-name return-value-type start-address end-address file-name

-

When fileName is specified, only the functions included in the specified file are displayed.

-

When fileName is not specified, then all the functions will be displayed.

Caution

This function uses the information displayed in the list of functions for program analysis.

[Example of use]

>>>project.GetFunctionList()
func1 int 0x00200 0x00224 C:\project\src\test1.c
func2 int 0x00225 0x002ff C:\project\src\test2.c
>>>project.GetFunctionList("C:/project/src/test1.c")
func1 int 0x00200 0x00224 C:\project\src\test1.c
>>>