B.3.8 CS+ Python property (for project)

Below is a list of CS+ Python properties (for a project).

Table B.8

CS+ Python Property (For Project)

Property Name

Function Description

project.Device

This property refers to the microcontroller of the active project.

project.IsOpen

This property confirms whether the project has been opened.

project.Kind

This property refers to the kind of the active project.

project.Name

This property refers to the active project file name (without path).

project.Nickname

This property refers to the nickname of the microcontroller of the active project.

project.Path

This property refers to the active project file name (with path).