A.1 Description

Below is a list of the panel related to the Python console.

Table A.1

Panel List

Panel Name

Function Description

Python Console panel

This panel is used to use IronPython to control CS+ and the debug tool via the command input method.