2.3.5  Delete a node locked license
 
In the License Manager window, select the license you wish to delete from the licenses area, then click the [Remove License] button to delete the license.
Figure 2.8  | License Manger Window  | 
 
 
Caution  | While an Upgrade (version) Node Locked License (permanent) is registered, the Node Locked License (permanent) that is the source of the upgrade cannot be deleted. Start by deleting the Upgrade (version) Node Locked License (permanent).  |