[All Messages] tab


This tab is used to display operation logs for all components (analysis tool, design tool, build tool, debug tool, etc.) provided by CS+.

Figure A.30

Output Panel: [All Messages] Tab

 

The following items are explained here.

[How to open]

-

From the [View] menu, select [Output].

[Description of each area]

(1)

Message area

This area displays operation logs for all components (analysis tool, design tool, build tool, debug tool, etc.) provided by CS+. Note that messages that the analysis tool output during analysis are not displayed on this tab (these messages are displayed only on the [Program Analyzer] tab).

The colors of message display differ with the type of message as shown below (character colors and background colors depend on the configuration in the [General - Font and Color] category of the Option dialog box).

Message Type

Display Example (Default)

Description

Normal message

 

Character color

Black

Displayed with information notices

Background color

White

Warning message

 

Character color

Blue

Displayed with warnings about operations

Background color

Standard color

Error message

 

Character color

Red

Displayed when there is a critical error, or when execution is not possible due to a operational mistake

Background color

Light gray

Remarks 1.

When the output message is double-clicked, or the [Enter] key is pressed with the caret over the message, the Editor panel appears and the destination line number of the file is displayed.

Remarks 2.

Help with regard to the message in the line is shown by selecting [Help for Message] in the context menu or pressing the [F1] key while the caret is in the line where the warning message or the error message is displayed.

Remarks 3.

You can save the contents displayed on this tab to a text file (*.txt) by selecting [Save Output-All Messages As...] from the [File] menu.