You can change the display order of the items (columns) displayed on the Function List panel/Variable List panel. There are two ways to perform this operation, as shown below.
There are two ways to perform this operation, as shown below.
(1) Performing the operation from the panel
(2) Performing the operation from the Column Chooser dialog box
Use the mouse to drag and drop the column name to move directly to an arbitrary column (header area).
On the left edge of the panel's header area, click the 
 button to open the Column Chooser dialog box, and then drag and drop the column names to move directly to the desired column (header area) on the panel using the mouse.