2.3.3 Output map information

The map information (the information of the link result) is output to the link map file.

Select the build tool node on the project tree and select the [Link Options] tab on the Property panel.

To output the link map file, set the [Output link map file] property in the [List] category.

(1)

Output information according to the output format

Select [Yes(List contents=not specify)(-LISt -SHow)] or [Yes(List contents=ALL)(-LISt -SHow=ALL)] in the [Output link map file] property.

Figure 2.15

[Output link map file] Property (When Information According To Output Format Is Output)

Remark

See "CC-RH Compiler User's Manual" for differences between the -SHow and -SHow=ALL options.

(2)

Specify information to be output

Select [Yes(List contents=specify)(-LISt)] in the [Output link map file] property. The following property will be displayed.

-

[Output symbol information] property

-

[Output number of symbol reference] property

-

[Output cross reference information] property

-

[Output total sizes of sections] property

-

[Output information of members of struct or union] property

-

[Output relocation attributes related to sections] property

-

[Output function list for detecting illegal indirect function call] property

 

Select [Yes] for each output information property.

Figure 2.16

[Output link map file] Property (When Information To Be Output Is Specified)

 

The link map file is output to the folder specified in the [Output folder] property in the [Output File] category.

It is also shown on the project tree, under the Build tool generated files node.

The file name will be the project file name with the extension replaced by ".map".

Remark

See "CC-RH Compiler User's Manual" for details about the link map file.