2.10.2 Combine multiple objects

For a multi-core project, the Intel HEX files or Motorola S-record files in the projects specified as constituent applications can be combined into a single hex file (This is called the object combine function).

Note that Intel HEX files and Motorola S-record files cannot be mixed.

(1)

Set the output of a hex file

Set the output of a hex file and the hex file format in the boot loader project and each application project.

Select the build tool node on the project tree and select the [Hex Output Options] tab on the Property panel.

Select [Yes] in the [Output hex file] property in the [Output File] category.

Figure 2.69

[Output hex file] Property

 

Select [Intel HEX file(-FOrm=Hexadecimal)] or [Motorola S-record file(-FOrm=Stype)] in the [Hex file format] property in the [Hex Format] category.

Figure 2.70

[Hex file format] Property

Caution

The same format should be selected in the boot loader project and all application projects.

(2)

Specify combining into a hex file

Specify combining into a hex file in the boot loader project.

Select [Yes] in the [Use object uniting function] property in the [Output File] category.

Figure 2.71

[Use object uniting function] Property

 

The destination where the combined hex file is to be output can be specified in [Output folder for united hex file] property (default: %BuildModeName%_merged).

The name in the [Output file name] property is used as the combined file name.