Specify Contents of Function Information dialog box


This dialog box is used to select the contents of function information and set it to the area that this dialog box is called from.

Figure A.10

Specify Contents of Function Information Dialog Box

 

The following items are explained here.

[How to open]

-

On the Property panel, select the following properties, and then click the [...] button.

-

From the [Link Options] tab, [Specify contents of function information] in the [Variables/functions information] category

[Description of each area]

(1)

[Select items]

The list of the contents of function information which can be specified for the area that this dialog box is called from is displayed.

Select the check boxes to specify the contents.

Item

Description

callt

#pragma callt is output for frequently called functions for the amount of surplus space remaining in the callt entry or near area.

near

#pragma near is output for frequently called functions for the amount of surplus space remaining in the near area.

rom_forbid

#pragma callt or #pragma near will not be output for functions in the section specified by the ROM option.

far_forbid

#pragma callt or #pragma near will not be output for functions in an absolute address section or a section specified as a far area by the -start option.

For details about each item, see the description of link option "-VFINFO" of "CC-RL Compiler User’s Manual".

Remark

In the area that this dialog box is called from, if the contents is already set, the check box for that contents will be selected by default.

[Function buttons]

Button

Function

OK

Closes this dialog box and sets the selected contents to the area that this dialog box is called from.

Cancel

Cancels the contents selecting and closes the dialog box.

Enable All

Selects all the check boxes in [Select items].

Disable All

Clears all the check boxes in [Select items].

Help

Displays the help of this dialog box.