The build speed-up facilities of this build tool are described here.
There are the following types of build speed-up facilities.
|
Multiple files are simultaneously passed by a single call of the build command. See "2.2.1 Running simultaneous build" for details about simultaneous build. |
|
|
Multiple build commands are executed in parallel. See "2.2.2 Running parallel build" for details about parallel build. |