1.2 Features

The features of the build tool plug-in are shown below.

-

Build option setting

Most build options can be set via the graphical user interface (GUI).

-

Speeding-up of build

Two types of facilities are provided to speed up build: simultaneous build and parallel build.

The build time can be shortened in simultaneous build by simultaneously compiling or assembling the files with a single call of the build command and in parallel build by executing multiple build commands in parallel.