Specify The Predefined Macro dialog box


This dialog box is used to select the predefined macros to disable and set it to the area that this dialog box is called from.

Figure A.10

Specify The Predefined Macro Dialog Box

 

The following items are explained here.

[How to open]

-

On the Property panel, select the following properties, and then click the [...] button.

-

From the [Compile Options] tab, [Invalidates the predefined macro] in the [Source] category.

-

From the [Individual Compile Options(C)] tab, [Invalidates the predefined macro] in the [Source] category.

-

From the [Individual Compile Options(C++)] tab, [Invalidates the predefined macro] in the [Source] category.

[Description of each area]

(1)

[Select items]

The list of the predefined macros which can be disabled for the area that this dialog box is called from is displayed.

Select the predefined macros to disable to set to the area that opened this dialog box, via check boxes.

Remark

In the area that opened this dialog box, if a predefined macros to disable is already set, the check box for that macro will be selected by default.

[Function buttons]

Button

Function

OK

Closes this dialog box and specifies the selected macros to the area that opened this dialog box.

Cancel

Cancels the macros selecting and closes the dialog box.

Enable All

Select all the macros in [Select items].

Disable All

Deselect all the macros in [Select items].

Help

Displays the help of this dialog box.