-r


This option outputs messages to the specified file.

[Specification format]

-r=file

 

-

Interpretation when omitted

Messages are output to the standard output file.

 

[Detailed description]

-

This option outputs messages to the specified file.

-

If the specified file already exists, it will be overwritten and no warning is output.

-

An error will occur if the specified file name matches the input or output file name of the C source file or C header file.

-

An error will occur if the parameter is omitted.

 

[Example of use]

>CcnvCA78K0  input.c  -o=output.c  -r=input.txt