Reads the results of A/D conversion (8 bits; most significant 8 bits of 10-bit resolution).
[Syntax]
#include r_cg_macrodriver.h
void R_ADC_Get_Result ( uint8_t * const buffer);
[Argument(s)]
I/O |
Argument |
Description |
O |
Uint8_t * const buffer; |
Pointer to area in which to store the results of A/D conversion |
Remark Below is an example of the results of A/D conversion to be stored in buffer.
![]() |
[Return value]
None.