Performs processing in response to detection of IICA slave communication error.
[Syntax]
#include r_cg_macrodriver.h
static void r_iican_callback_slave_error ( MD_STATUS flag );
Remark n is the channel number.
[Argument(s)]
|
I/O |
Argument |
Description |
|
I |
MD_STATUS flag; |
Cause of communication error MD_ERROR: Address mismatch detected MD_NACK: Acknowledge not detected (Master receiving end) |
[Return value]
None.