Operates the signed multiply.
[Syntax]
#include r_cg_macrodriver.h
#include r_cg_mac32bit.h
void R_MAC32Bit_MULSigned ( int32_t data_a, int32_t data_b, mac32bit_int64_t
* buffer_64bit );
[Argument(s)]
|
I/O |
Argument |
Description |
|
I |
int32_t data_a; |
Multiplicand |
|
I |
int32_t data_b; |
Multiplier |
|
O |
mac32bit_int64_t * buffer_64bit; |
Multiplier result |
Remark Below is an example of the structure mac32bit_int64_t for the multiplier result.
|
typedef struct { int16_t low_low; int16_t low_high; int16_t high_low; int16_t high_high; } mac32bit_int64_t; |
[Return value]
None.