Reads the alarm conditions (year, month, weekday, day, hour, minute, second).(in the case of the calendar mode setting)
[Syntax]
#include r_cg_macrodriver.h
#include r_cg_rtc.h
void R_RTC_Get_CalenderAlarmValue ( rtc_alarm_value_t * const alarm_val );
[Argument(s)]
|
I/O |
Argument |
Description |
|
O |
rtc_alarm_value_t * const alarm_val; |
Pointer to structure in which to store the conditions being read |
Remark See R_RTC_Set_AlarmValue for details about rtc_alarm_value_t (alarm conditions).
[Return value]
None.