Usage example

Start data transfer by the end of A/D conversion.

(Get A/D conversion results of 4 pins and copy them to RAM. Then, calculate the average of the results.)

[GUI setting example]

DMA controller

Used

DMA0

Used

DMAoperation setting

Used

Transfer direction setting

SFR to internal RAM

Transfer data size setting

8 bits

SFR address

ADCR - 0x000fff1e

RAM address

0xffe00

Transfer byte count

4

Trigger signal

INTAD (Please set INTAD)

DMA0 transfer end interrupt (INTDMA0)

Used

Priority

Low

A/D convertor

Used

ADC

Used

A/D convertor operation setting

Used

Comparator operation setting

Operation

Resolution setting

8 bits

VREF(+) setting

VDD

VREF(-) setting

VSS

Trigger mode setting

Software trigger mode

Operation mode setting

Countinous select mode

ANI0 - ANI7 analog input selection

ANI0 - ANI3

A/D channel selection

ANI0 - ANI3

Conversion time mode

Normal 1

Conversion time

34 (1088/fCLK)(μs)

Conversion result upper/lower bound value setting

Generates an interrupt request (INTAD) when ADLL≦ADCRH≦ADUL

Upper bound (ADUL) value

255

Lower bound (ADLL) value

0

Use A/D interrupt (INTAD)

Used

[API setting example]

r_main.c

void main(void)

{

R_MAIN_UserInit();

/* Start user code. Do not edit comment generated here */

/* Enable DMA0 transfer */

R_DMAC0_Start();

/* Start the AD converter */

R_ADC_Start();

while (1U)

{

NOP();

}

/* End user code. Do not edit comment generated here */

}

r_cg_dmac_user.c

/* Start user code for include. Do not edit comment generated here */

#include "r_cg_adc.h"

/* End user code. Do not edit comment generated here */

/* Start user code for pragma. Do not edit comment generated here */

#pragma address (g_adc_buf = 0x0ffe00)

/* End user code. Do not edit comment generated here */

/* Start user code for global. Do not edit comment generated here */

volatile uint8_t g_adc_buf[5][4];

volatile uint8_t g_adc_buf_cnt = 0U;

/* End user code. Do not edit comment generated here */

static void __near r_dmac0_interrupt(void)

{

/* Start user code. Do not edit comment generated here */

uint8_t i;

uint8_t j;

uint16_t temp;

/* Stop the AD converter */

R_ADC_Stop();

/* Disable DMA0 transfer */

R_DMAC0_Stop();

/* Change DMA0_RAM address */

if ((++g_adc_buf_cnt) < 4U)

{

DRA0 += 4U;

}

else

{

DRA0 = _FE00_DMA0_RAM_ADDRESS;

g_adc_buf_cnt = 0U;

/* Calculate the average */

for (i = 0; i < 4U; i++)

{

temp = 0U;

for (j = 0; j < 4U; j++)

{

temp += g_adc_buf[j][i];

}

g_adc_buf[4][i] = temp / 4U;

}

}

/* Enable DMA0 transfer */

R_DMAC0_Start();

/* Start the AD converter */

R_ADC_Start();

/* End user code. Do not edit comment generated here */

}