Perform toggle operation at fixed intervals and output a suquare wave with a duty factor of 50%.
[Waveform example]

[GUI setting example]
|
Timer |
Used | |||
|
TAU0 |
Used | |||
|
Channel0 |
||||
|
channel 0 |
Square wave output | |||
|
Square width |
100μs (Actual value:100) | |||
|
Generates INTTM00 and inverts timer output when counting is started |
Unused | |||
|
Initial output value |
0 | |||
|
End of timer channel0 count, generate an interrupt (INTTM00) |
Used | |||
|
Priority (INTTM00) |
Low | |||
[API setting example]
r_main.c
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Start TAU0 channel 0 counter */
R_TAU0_Channel0_Start();
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}