Overview

Below are the naming conventions for API functions output by the Code Generator.

- Macro names are in ALL CAPS.

The number in front of the macro name is a hexadecimal value; this is the same value as the macro value.

- Local variable names are in all lower case.

- Global variable names start with a "g" and use Camel Case.

- Names of pointers to global variables start with a "gp" and use Camel Case.

- Names of elements in enum statements are in ALL CAPS.