r_cmpc_cmpcn_interrupt

Performs processing in response to the comparator C interrupt.

Remark This API function is called to run interrupt processing for the comparator Cn interrupt, which is generated when the comparison result changes at this time.

[Syntax]

static void r_cmpc_cmpcn_interrupt ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.