R_CRC_Get_Result

Gets the result of operation.

[Syntax]

void R_CRC_Get_Result ( uint16_t * const result );

void R_CRC_Get_Result ( uint32_t * const result );

[Argument(s)]

I/O

Argument

Description

O

uint16_t * const result;

Pointer to the location where the result of operation is stored

I/O

Argument

Description

O

uint32_t * const result;

Pointer to the location where the result of operation is stored

Remark The size of argument differs for each device group.

[Return value]

None.