r_dmac_dmacni_interrupt

Performs processing in response to the transfer end interrupt.

Remark The API function is called as the interrupt process corresponding to the DMA transfer end interrupt for channel n

[Syntax]

static void r_dmac_dmacni_interrupt ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.