R_DOC_WriteData

Sets the value for comparison with, addition to, or subtraction from the reference value.

[Syntax]

void R_DOC_WriteData ( uint16_t data );

[Argument(s)]

I/O

Argument

Description

I

uint16_t data;

Input data for use in operation

[Return value]

None.